Reliable energy supply to the robot arm in milking system during continuous operation

Robust energy chains are used in milking systems when ammonia levels are high.

24-hour operation, fluctuating temperatures and air containing ammonia - the cowshed conditions with which technical components of automatic milking systems also have to cope are not easy. In order to be able to rely on safe function, the GEA company relies on harnessed energy supply solutions from igus for its products.

Profile

  • What was needed: E2/000 series energy chains and chainflex cables, supplied as a completely pre-assembled readychain system
  • Requirements: the system must withstand conditions such as 24-hour operation, fluctuating temperatures and ammonia-containing air levels
  • Industry: agricultural industry, milking system
  • Success for the customer: thanks to a pre-assembled system from igus, the customer received everything from a single source and was able to make savings in the procurement process, the energy chains ensure high availability and are protected in the system from external influences
MIone milking system When an animal enters a box of the MIone milking system, the milking process starts fully automatically.

Problem

Starting, cleaning, stimulating, pre-milking, milking - these are the individual steps that the MIone, an automatic milking system from GEA Farm Technologies GmbH, carries out independently as soon as an animal lines up at the box.
The system from the mechanical engineering company has already been in volume production for several years and is used for herd sizes from about 70 animals upwards. The special thing about the MIone is that the cows themselves decide when they should go for milking. The animals simply line up at the free box, which is detected by the system and the automatic process is initiated. A robot arm is extended and the individual teat cups at the end of the arm are placed on the udder teats one by one with pinpoint accuracy. The system works quietly while the animal is busy eating. After the entire milking process is completed, the teat cups detach from the udder, are cleaned and prepared for the next cow. The challenge for these systems is the 24-hour operation and the wide variety of conditions that can prevail in the barn. These are, for example, fluctuating temperatures from 0°C to 40°C, usually high humidity as well as air that often contains ammonia. This also affects all individual components of the MIone .

Solution

The energy supply to the robot arm is implemented with polymer energy chains and cables from igus, for which these conditions do not present any great difficulties. Specifically, two E2/000 series energy chainsfilled with chainflex cables specially developed for movement are used. One chain travels on the horizontal and one on the vertical axis. For some years now, GEA has also been procuring the e-chains as completely pre-assembled readychains, which enables savings in the procurement process.
The dynamics are relatively low in the application of the MIone, which is important so as not to injure the animals. Due to the protected installation of the energy chains in GEA's machines, damage caused by external influences can be virtually ruled out. However, operational reliability and high availability are all the more crucial. All facilities must function around the clock, unplanned stoppages are to be avoided at all costs. When the machine specialist designed the cables for the application together with igus, the cycles were estimated for ten years and the requirements were determined exactly. Since both the energy chains and the cables are supplied from a single source, it is possible to match them optimally. This creates additional security for the customer.
 
MIone with energy chains In GEA's MIone, two energy chain systems from igus are used in each case - one system in the horizontal and one in the vertical.
GEA with energy chain GEA purchases the energy chains and cables as fully-harnessed readychains.

motion - magazine for energy chain systems®

Improve the performance of your machine ... Cost down.

In this igus® magazine you will find numerous possibilities and application examples of how you can bring your tech up and/or cost down with ready-to-install energy chain systems.
Order your personal copy here

Danışma

Sorularınızı şahsen yanıtlamaktan mutluluk duyarım

Nakliye ve danışmanlık

Şahsen:

Pazartesi-Cuma, sabah 7 - akşam 8 arası.
Cumartesi sabah 8 - akşam 12 arası.

Online:

24h


"Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" ve "yes" terimleri, igus® GmbH/ Köln'ün Federal Almanya Cumhuriyeti'nde ve bazı yabancı ülkelerde yasal olarak korunan ticari markalarıdır. Bu liste, igus GmbH'nin veya igus'un bağlı şirketlerinin Almanya, Avrupa Birliği, ABD ve/veya diğer ülkeler veya yargı bölgelerinde korunan ticari markalarının (örn. bekleyen ticari marka başvuruları veya tescilli ticari markalar) kapsamlı olmayan bir listesidir.

igus® GmbH, Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber şirketlerinin ve bu web sitesinde adı geçen diğer tüm tahrik üreticilerine ait hiçbir ürünün satışını yapmadığını ifade etmektedir. igus® tarafından sunulan ürünler, igus® GmbH'nin ürünleridir.