Plastic energy chain for safe cable guidance on a 2000HP jack-up rig

Robust E4.1 e-chains are used for the cantilever and drill floor skid on this drilling vessel.

This jack-up rig was equipped with our E4.1 e-chains from the 800 and E4.112 series with an extension link for high additional loads. The reverse energy chain principle for the cantilever and the gliding extension link chain on the drill floor reduce the installation space required for the system. The low energy chain support distance means that all cable diameters can be safely guided. This is reflected in a fail-safe, maintenance-free system.

Profile

  • What was needed: E4.1 series energy chains
  • Requirements: On a jack-up rig, a strong, fail-safe solution was needed for cable guidance for the cantilever and drill floor skid. Since there was little installation space, the solution was also to be as space-saving as possible.
  • Industry: Oil and gas
  • Success for the customer: E4.1 energy chains created a fail-safe, maintenance-free cable guidance system. With its reinforced extender crossbar design, the e-chain safely guides the heavy cable packages. And the low support distance ensures safe guidance for cables of all diameters.
Offshore energy chain Emphasis on robustness: Designed as a strong extension link chain, the plastic E4.1 energy chain ensures reliable cable guidance on the drilling vessel.

Problem

Jack-up rigs are used as modular drilling rigs (MDRs) to transport additional drilling equipment to fixed drilling platforms. Once at the drilling site, the drilling vessel's legs extend to the seabed and provide support to then raise the drilling floor to the level of the drilling platform. A cantilever is positioned above the drilling site, and drilling can begin.
For this jack-up rig, suitable cable guidance to the cantilever and the drill floor was sought during the planning stage. The solution had to bear the high additional cable load continuously and without failure. The installation also required a system that was as space-saving as possible. The tight installation space required compact but secure bundling of all cables.

Solution

High additional loads, robust cable guidance, and compact installation. With these requirements, the manufacturer started looking – and found the solution in our E4.1 series energy chains. The 800 and E4.112 versions are used. The particularly robust cable guidance systems from the heavy duty range were chosen due to the large, heavy cable packages. To move safely with loads, they were designed as extension link chains, that is, as a reinforced system. The low support distance for both systems also means that all cable diameters can be safely guided. This is ultimately reflected in a fail-safe, maintenance-free system.
Offshore energy chain One requirement for using the e-chain in the rig was that it move the heavy cable weight safely over the long term.
Offshore energy chain The large energy chain is clearly visible on the side of the cantilever. It moves with the drill floor skid.

Here you can find the products used

800 series

Inner height hi: 200mm
Inner widths Bi: 200-600mm
Bend radii R: 325-1000mm
Pitch: 250mm

E4.112 series

Inner height hi: 112mm
Inner widths Bi: 50-600mm
Bend radii R: 200-1000mm
Pitch: 143mm


"Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "tribotape", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" ve "yes" terimleri, igus® GmbH/ Köln'ün Federal Almanya Cumhuriyeti'nde ve bazı yabancı ülkelerde yasal olarak korunan ticari markalarıdır. Bu liste, igus GmbH'nin veya igus'un bağlı şirketlerinin Almanya, Avrupa Birliği, ABD ve/veya diğer ülkeler veya yargı bölgelerinde korunan ticari markalarının (örn. bekleyen ticari marka başvuruları veya tescilli ticari markalar) kapsamlı olmayan bir listesidir.

igus® GmbH, Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber şirketlerinin ve bu web sitesinde adı geçen diğer tüm tahrik üreticilerine ait hiçbir ürünün satışını yapmadığını ifade etmektedir. igus® tarafından sunulan ürünler, igus® GmbH'nin ürünleridir.