Güzeller Org. San. Bölg. Galvano
Teknik San. Sit. Cumhuriyet Cad. 2/32
P.K. 41400 Gebze / Kocaeli
For this, Messer's technicians in Brazil worked closely with igus to develop a design in which the e-chains were nested inside each other. This reduced the installation space and ensured safe guidance of the cables and hoses. Here, the e-chains of the series 3500 with 150 mm and 250 mm bend radius were used. An autoglide system ensures that the chains slide straight over each other. Due to the special comb-like crossbars, the chain basically guides itself, which means there is no need for an additional guide trough. e-chain systems from igus are made of high-performance polymers and can easily withstand the aggressive ambient conditions. In addition, according to Maxwell Santos of Messer, one of the particular technical and economic advantages of igus products is the cost savings: "The energy chains basically cost half as much because they last twice as long," explains the technical director. In the long term, igus energy chains are the most economically efficient solution for Messer as they are maintenance-free and have a long service life, which lead to cost savings and significant productivity gains for its customers. "We have never had any problems with igus as a supplier", adds Maxwell Santos. "They function without any failures and unplanned downtimes. Apart from the technical properties of the e-chains, the support service provided by igus and trust in the product information were decisive factors for Messer. This strengthened the partnership during development of the project over a period of years. This partnership extends worldwide as Messer uses igus energy chains in plants in Germany, the United States, India and China alongside Brazil. No better solution could be found at any of its five locations.
Pazartesi-Cuma, sabah 7 - akşam 8 arası.Cumartesi sabah 8 - akşam 12 arası.
24h