Güzeller Org. San. Bölg. Galvano
Teknik San. Sit. Cumhuriyet Cad. 2/32
P.K. 41400 Gebze / Kocaeli
Even if iglidur plain bearings have been developed for lubrication-free applications, they can of course be used with additional lubricants - for example, in hydrodynamic and hydrostatic plain bearings. Find out here exactly how these two types of plain bearing work, what advantages they have and where they are used.
A hydrodynamic plain bearing is a type of bearing in which there is minimal clearance between bearing and shaft. This gap is filled with lubricant. When not in use, the shaft rests on the plain bearing.
When the shaft starts to rotate, lubricant is drawn into the narrow space between the bearing and shaft and the pressure in the lubricant increases the faster the shaft rotates. This forms a so-called lubrication wedge underneath the shaft, lifting it up. As a result, plain bearing and shaft are no longer touching as they are separated by a lubricating film.
Hydrodynamic plain bearings are frequently found in the automotive industry , where they are used in thermal management. They are also common in ships and submarine turbines as they operate with optimum performance in humid environments. They also play an important role in energy generation, especially in wind turbines and hydroelectric power stations. Hydrodynamic plain bearings are also used in industrial machinery, such as large machine tools and pumps. Their ability to carry high loads with low friction makes them ideal for these applications.
A hydrostatic plain bearing is a type of bearing in which a pump is used to insert lubricant between the shaft and the bearing. In contrast to hydrodynamic bearing positions, this type is therefore permanently fully lubricated.
Hydrostatic plain bearings are used when a centric operation of the shaft is required. However, as the oil supply or oil pressure poses a safety risk, hydrodynamic bearings are generally favoured.
Hydrostatic plain bearings have areas of application similar to those of hydrodynamic plain bearings. However, as they have a higher true-running accuracy, they are often found in high-precision applications, such as measuring machines or machine tools. Just like hydrodynamic plain bearings, they are also used in power generation. Here, they form part of turbines and generators, among other things.
igus offers various plastic bearings that can be combined with hydrodynamic lubrication. Their main differences are the application parameters, such as temperature or chemical resistance, for which they have been developed.
See for yourself the quality of our products. The iglidur improves sample box contains:
✅ 39 iglidur plain bearings made from the most important materials